I am trying to understand the data transfer between the SERCOS drives in our Indraworks program over to our Allen Bradley PLC program. The biggest thing I am confused about is how you set up the starting point for the signal status and signal control words. The "C3_Bosch_Unload..." is the name of the Ethernet module card. You can see from the attached pictures that M187_1 and M187_2 are higher up in the project Explorer Tree in the Indraworks program, but are further down the array tag "C3_Bosch_Unload:I.Data" in the Allen Bradley program. M183 is further down the project explorer tree in the Indraworks program, but is higher up in the "C3_Bosch_Unload:I.Data". How is the starting point set for where these data values are going to be in the Allen Bradley array tag?