IndraDrive and DKC11.3 drive

Hello,

I'm pretty new to Rexroth drives, but i have to parametrize DKC11.3 controller.
I already sucesfully connected via USB to RS232 converter to the drive from IndraDrive, but i can't see any paratemers or axis. If i tried search parameters it shows parameters, but when i try to open the parameter it shows error IDN not available.
In the menu tree i can see a file icon with "drive" name and in the left down corner it shows the COM port and baud rate, so i assume i'm connected to the drive, because with other baud rates it shows nothing...

What i have to do to be able to see a parameters and set them?

Best reply by JordiLaboria
View original
3 replies