HCS01 settings for 110V

We are commissioning a machine with a HCS01.1E-W0006-A-02-B (single phase) drive with MPB-20VRs in Germany and want to ship this machine to the Canada. Which Parameters do we have to adjust to fit the local 110V grid?

Thank you in advance.

Best reply by ilya

Hello Michael,

HCS01.1E-W0006-A-02-B supports 110V as is. Keep in mind that 110V single phase will yield a lower DC bus voltage than what you are testing with in Europe (220V, I assume) so the torque performance might decrease relative to the motor speed. It depends how fast you are running this motor. I recommend to consult the torque/speed charts on 220V and 110V to see the difference after measuring the torque/speed feedback on the test machine in Europe.

Good luck.

ilya

View original
1 reply