Configuration of Indra Drive Cs in velocity control

Helo, i am new to servo drives. I have following controller and servo drive
Controller : HSC01.1E.W0018-A-03-B-ET-EC-NN-NN-NN-FW
Motor : MSK040C-0600-NN-S1-UP0-NNNN
I have run the motor in easy startup mode but can't configure the drive in Velocity mode. When ever i try to configure the S-0-0032 parameter it gives error. Can any one guide to which parameters are related to velocity control so that if i am missing on i can correct it. Any help would be greately appreciated.
17175757748165407650520573044809.jpg
4.2MB
3 replies