Export/import functionality

I got a HELIO project from a college and I would like to export several pages etc. from this template project to my existing project. I can't find a import functionality. It should be possible to do a export of a whole or only parts of a project. And on import side it should be possible to make selections what should be imported from the export.

The only thing I found is copy & paste single objects, like a page. But this is very unfriendly, unless one has two ctrlX CORE (real or virtual). Then copy & paste could be enough.

Best reply by HmiGuide

Since only one project is supported on the ctrlX, copying and pasting is cumbersome.

Option 1: Open projects sequentially

  • Open Project A,

  • Copy the element,

  • Close Project A

  • Open Project B

  • Paste the element

Option 2: Open projects on two ctrlX devices

  • Open Project A on ctrlX A

  • Open Project B on ctrlX B

  • Paste the element between the two projects

My idea to use the Windows clipboard history (Windows key + V) doesn't work, because the values ​​copied with Ctrl+C are not entered there.

View original
1 reply