Hello everyone,
I have got problem with connection of the ctrlX SafeX C.12 to the CtrlX Core.
I saw two posts LINK1 and LINK2 but I still can't get rid of my problem.
I have got the ctrlX IO Engineering WRK-V-0116 and ctrlX SAFETY Engineering 1.7.1.8233 versions. I have also uploaded the SafeX .XML file to the ctrlX IO (2022-09-01 version).
I tried to add SafeX C.12 both ways:
1. by scanning for the devices
2. by adding the device from offline database
Then, in both situations I uploaded the configuration to the CtrlX Core and then the problem occurs. There is an error "0x001E: Invalid Input Configuration". Slave can't go in to OP mode.
Is there any solution for this problem?
Thank you in advance for your help.
Best wishes, Filip
ย