Ethernet IP communication hand-shaking between AB plc and Core at power up

Hello,

one of our customers is in commissioning their machine using a CtrlX core with three CtrlX drives controller by AB plc. the machine is showing the functions, but they have some issues.

one of the issues is the core taking longer time to start-up than AB plc. they want to have a hand-shaking signal back to AB PLC to show the core is in operation mode, the drives in OM mode and the motion is ready. the PLC app can check the drive status (P115), but is there a way to confirm all apps are running and ready in the PLC app? sometimes the updates of status are slow. that is another issue.

second issue is they got a lot of acceleration/deceleration limits exceeded warning. the set value of accel was 200mm/s^2 and the limit was 10m/s^2. while one axis was stand still and another axis was touching the first one, but the speed was not high. I will have the customer to double check if the accel was actually over the limit.

anyway, your help is highly appreciated!ย 

ย 

Best reply by Jesse

sorry for the late response. we got some help from the development group and found out the reason why it didn't work. it was an encoder port assignment issue since the motor is MSK. you can close this topic now. Thanks,ย 

View original
4 replies