Using a kinematic with four Axis (three linear, one rotational only in positive direction) in IDE

Hello everyone,

i want to create a kinematic with four Axis and use it in the IDE. Three of these Axis are the X, Y and Z-Axis of a cartesian motion system. The fourth is for the engine of an application applied to the z-Axis. This engine only spins in positive direction and is not a swing axis.

How can i make this configuration work? I already get an error in the motion when i try to group it after turning the power on.

Thank you šŸ™‚

Best reply by CodeShepherd

All axes that are part of a kinematic are moved coordinated. That means the movements starts and stops at the same time. The set velocity in a kinematic command is only affecting the TCP path. (See motion object documentation) So the velocity of the 4th axis will result from the time needed to complete theĀ command for all axes and the commanded distance. Please also beware of the motion limit values of the axes.

The direction of rotation isĀ determined by your commanded position.

If you just like to like to run a rotational axis freely at the same time as the kinematic I would suggest to do a parallel single axis command for it. In the IDE you can choose run in parallel. The mane problem here is when your axis movementĀ should stop.

We couldĀ also have a live meeting to get a better idea what you want to do and how to reach it. Please write me a personalĀ message with your contact data to do so.

Ā 

Ā 

View original
3 replies