Hi,
I am trying to enable "Enabling IP Forwarding" in the tun0 settings once I have a VPN connection to an OpenVPN instance. It is this setting:
As soon as I click "Save" I get this configuration error, but no other information:
Â
There is no fault or information in the log files. Everything else seems to be working with the VPN app but I need this option to allow access to other devices on the same local network as the ctrlX CORE. I would like to forward IP Addresses on the main engineering port of the ctrlX CORE that has a fixed IP address on a local network switch. I granted the user all permissions that I could find that were related to the function, tried rebooting too, but it didn't work. Additionally, the "Use External Settings" option is never available.
Can you provide more information about this config error and how to enable "Use External Settigns"?
Connections: XF10 - Fixed IP, connected to local network switch. XF51 - DHCP, connected to internet connection, connected to OpenVPN account. IndraDrive - fixed IP on X26, connected to local network switch, same subnet as XF10.
Thanks!