08/05/2025
ctrlX CORE | Vision | USB | Camera | OpenCV | Python

Python snap to stream USB webcam images to ctrlX Data Layer

Idea

This How-To will walk you through the process of connecting a USB webcam to the ctrlX CORE for simple vision applications, without the need for an industry-standard camera. You will have to build your own Python Snap to capture images, encode them as Base64-JSON strings, save them to a Datalayer node, and finally allow Node-RED to display the images on a dashboard. While there is no guarantee that this will work with your specific camera, it was successful with the one I had on my desk.

What you need

Overview

  • A Datalayer Provider handles the Datalayer node for the webcam image data.

  • A Datalayer Client App

    • ... finds the USB webcam within /dev/video*

    • ... captures images with the Python library OpenCV

    • ... encodes them as Base64-JSON-strings

    • ... writes them to the specified Datalayer Node

  • Node-RED can subscribe to the Datalayer Node and display the image stream on a dashboard

Step by Step

Datalayer Provider

First you will need a Datalayer provider snap, that creates a node for the webcam images. I used the python sample datalayer.provider from the Software Development Kit (SDK) and adjusted it a bit to get the Datalayer node seen below.

Datalayer node for webcam data

Datalayer Client with Webcam handling

Next, take the sample datalayer.client.simple and add all the needed webcam functionality. Therefore, please download webcam.py at the end of this article and upload it into your SDK build environment.

part of webcam.py

The class Webcam is implemented with the python vision library OpenCV. The code won't be discussed here as it should be self explanatory if you have a look at it.

Inside your main.py add the following lines of code at the designated locations:

from ctrlxdatalayer.variant import Variant 
from helper.webcam import Webcam

def main():
    ...
    # get webcam access
    cam = Webcam()

    ...

            while datalayer_client.is_connected() and not __close_app:
                
                # get image from webcam
                imageJsonString = cam.get_frame_json()

                # write to datalayer
                data = Variant()
                data.set_string(imageJsonString)
                addr = "sdk/webcam/image/"
                result, var = datalayer_client.write_sync(addr, data)

                time.sleep(0.1)

If you want to adjust the frames per second, that you will stream to the Datalayer, adjust the time.sleep(...) value to your needs.

Next add the required plugs and packages to the snapcraft.yaml file:

apps:
  client:
    command: bin/main.py
    plugs:
      - network
      - datalayer
      - camera
      - hardware-observe
    daemon: simple
    restart-condition: always
    passthrough:
      restart-delay: 10s

parts:
  client:
    plugin: python
    source: .
    stage-packages:
      - ctrlx-datalayer
    python-packages:
      - opencv-python-headless

Finally edit setup.py according to your snap name and the required packages.

After you build the snap successfully and install it on your ctrlX CORE, you should see the Base64-JSON-string output of your snap inside the specified Datalayer node similar to the image seen earlier in the article.

Node-RED Dashboard

To display the webcam stream in a Node-RED dashboard you simply have to add three nodes:

  • Data Layer Subscribe

  • json (converts the JSON string to a JSON object)

  • template (from Dashboard, not Dashboard 2.0)

Node-RED flow

Inside the template node insert:

<div>
    <img
    id="cam"
    ng-src="data:image/{{msg.payload.format}};base64,{{msg.payload.image}}"
    style="max-width: 100%; height: auto;"
    onload="
      const img = document.getElementById('cam');
      document.getElementById('res').innerText = img.naturalWidth + '×' + img.naturalHeight;
    "
  />
    <div id="res" style="text-align: center; margin-top: 8px;"></div>
</div>

To be able to see your webcam stream at a faster refresh rate than 1 frame per second, go to the configuration nodes via the dropdown menu in the upper right corner (1), open the ctrlx-config-subscription node (2), set the Publish and Sampling Interval (3) (the default value is 1 second) and finally hit Update (4).

After you hit deploy, you should be able to see the webcam stream in the Node-RED Dashboard.

Node-RED Dashboard

5
webcam.zip
3.53KB
Types
How-to
Products
Controls
Markets
Assembly Lines
Building Automation
Logistic
Packaging
Production Machines