This How-To describes the required preparation to replace a ctrlX CORE without the need of using an engineering PC.
The PC-less device replacement requires a prior preparation, while the ctrlX CORE is still running the target application.
Too late? Your device is not available anymore, then read about hardware reset.
PrerequisitesPrepare version independence (recommended)Possibility 1: PC-less device replacement via license dongle µSD card (ctrlX CORE X3 only)Create backup file on license donglePrepare the backup-file on license dongle µSD cardReplace your device, PC-lessPossibility 2: PC-less device replacement via license dongle µSD card and USB stick (all ctrlX CORE variants)Create backup file on the USB stickPrepare the backup-file on the USB stickReplace your device, PC-lessRelated information
Prerequisites
ctrlX CORE X3/X5/X7 is running and in operation the target application
Engineering PC is connected to the ctrlX CORE
User is logged in ctrlX OS web UI with administration rights
A license dongle (SD card) with required licenses for the application is plugged in ctrlX CORE
An USB stick minimum 4 GB and maximum 32 GB, formatted as FAT32
For ctrlX COREplus X5/X7: only including one GPT partition (GUID partition table). See "How to partition a disk as GPT & Restore ctrlX CORE X7".
Current application is based on ctrlX OS >= 3.6
Prepare version independence (recommended)
The replacement ctrlX CORE already has to have system major version 3.x already installed if the backup restoration mechanism should be used only! To get version independent and also save a lot of time while restoration process, a system image has to be added to the corresponding USB device. More information see online documentation "Hardware reset".
Download the corresponding system image via the Collaboration Room
Connect the external data carrier to the engineering PC
Unzip the archive to the external data carrier
X3: "X3_Systemimage_x.x.x.zip" to the license µSD card or USB Stick
X5 and X7: "X5_X7_Systemimage_x.x.x.zip" to the USB stick
To prevent restoring the image to the same control
Create directory /rescue/<serial number of control>
There create a file .done (e.g. /rescue/726xxxxxxxxxx/.done)
Possibility 1: PC-less device replacement via license dongle µSD card (ctrlX CORE X3 only)
The PC-less device replacement only using the license dongle µSD card, is available for ctrlX CORE X3, ctrlX COREplus X3 and drive integrated ctrlX CORE X3.
Please check (again! 😜) the chapter "Prerequisites" before continuing.
The current device settings are put onto and the required licenses are assigned to the license dongle.
Create backup file on license dongle
In the ctrlX OS webUI: Open the “Settings” window and click on the tile “Storage”
ctrlX OS web UI - open setting "Storage" Mount µSD card via corresponding button
ctrlX OS web UI - mount µSD card Open the “Settings” window and click on the tile “Backup & Restore”
ctrlX OS web UI - open "Backup & Restore" Click on the “Backup” tile
ctrlX OS web UI - open "Backup" Enter/check backup setting:
Select the device settings and resources to be added to the backup file (default all data is selected)
Select the license dongle µSD card in the "Backup file storage"
Tick setting "Force reboot after restore" in "Additional settings", so control will end up in OP after restoration
Enter a password e.g. "secret" (mandatory to store the device certificates)
ctrlX OS web UI - create backup on µSD card Click on the “Create”
A backup file [yyyy-mm-dd-XX-XX-XX_ctrlx-backup.zip] will be generated
Prepare the backup-file on license dongle µSD card
Open the file browser of the license dongle µSD card via “Settings” window and click on the tile “Storage”, then click "Open file browser"
ctrlX OS web UI - open file explorer of µSD card To confirm that the backup file should be used for restoration:
Rename the backup file to [yyyy-mm-dd-XX-XX-XX_ctrlx-setup.zip]Create a file "setup.options.json"
Write password of the backup archive inside file "setup.options.json"
{ "$password": "secret" }To prevent restoring the backup to the same control, create a file "setup.<IP of control>.done" (e.g. /setup.726xxxxxxxxxx.done)
Your done! The license dongle can remain in the ctrlX CORE during operation.
Replace your device, PC-less
The device is defect? Too bad!
Replace the defect device through a replacement ctrlX CORE
Remove the license dongle from the defective device
Insert license dongle into the replacement devices µSD slot
Switch on the replacement device: The backup file will be recovered automatically
[callout type="warning" headline="DO NOT REMOVE POWER DURING UPDATE!" text="While update, the ctrlX CORE is restarted multiple times and the operating system is initialized for the first time. The entire update, including an initial initialization, can take several minutes!"]The new ctrlX CORE is ready and will boot up to operation!
[callout type="info" text="Apps that are already installed in the correct version will be skipped during restoration.On first login there could be a warning showing possible errors during restoration. See file "setup.log" on the µSD card for restoration details."]
Possibility 2: PC-less device replacement via license dongle µSD card and USB stick (all ctrlX CORE variants)
The PC-less device replacement via license dongle µSD card and USB stick is available for all variants of the ctrlX CORE device.
Please check chapter "Prerequisites" before continuing.
The current device settings can be saved to a backup file and stored on the USB stick. The required licenses are assigned to the license dongle.
Create backup file on the USB stick
In the ctrlX OS webUI: Open the “Settings” window and click on the tile “Storage”
ctrlX OS web UI - open setting "Storage" Mount USB stick via corresponding button
ctrlX OS web UI - mount USB stick Open the “Settings” window and click on the tile “Backup & Restore”
ctrlX OS web UI - open "Backup & Restore" Click on the “Backup” tile
ctrlX OS web UI - open "Backup" Enter/check backup setting:
Select the device settings and resources to be added to the backup file (default all data is selected)
Select the USB stick in the "Backup file storage"
Tick setting "Force reboot after restore" in "Additional settings", so control will end up in OP after restoration
Enter a password e.g. "secret" (mandatory to store the device certificates)
ctrlX OS web UI - create backup on USB stick Click on the “Create”
A backup file [yyyy-mm-dd-XX-XX-XX_ctrlx-backup.zip] will be generated
Prepare the backup-file on the USB stick
Open the file browser of the USB stick via “Settings” window and click on the tile “Storage”, then click "Open file browser"
ctrlX OS web UI - open file explorer of USB stick To confirm that the backup should be used for restoration:
Rename the backup file to [yyyy-mm-dd-XX-XX-XX_ctrlx-setup.zip].Create a file "setup.options.json"
Write password of the backup archive inside file "setup.options.json"
{ "$password": "secret" }To prevent restoring the backup to the same control, create a file "setup.<IP of control>.done" (e.g. /setup.726xxxxxxxxxx.done)
Your done! The USB stick and the license dongle can remain in the ctrlX CORE during operation.
Replace your device, PC-less
The device is defect? Too bad!
Replace the defect device through a replacement ctrlX CORE
Remove the USB stick and license dongle from the defective device
Insert license dongle into the replacement devices µSD slot
Plug the USB stick into the XF01C slot of the ctrlX CORE
Switch on the replacement device: the backup file will be recovered automatically
[callout type="warning" headline="DO NOT REMOVE POWER DURING UPDATE!" text="While update, the ctrlX CORE is restarted multiple times and the operating system is initialized for the first time. The entire update, including an initial initialization, can take several minutes!"]The new ctrlX CORE is ready and will boot up to operation!
[callout type="info" text="Apps that are already installed in the correct version will be skipped during restoration.On first login there could be a warning showing possible errors during restoration. See file "setup.log" on the USB Stick for restoration details."]