02/14/2025
Koch | Energy Management | Safety

How to layout, size and connect Koch Bremsenergie (Koch Brake Energy) modules to ctrlX DRIVE

Introduction

The Koch Bremsenergie (Koch Brake Energy) module is an energy management module which provides several advantages and safety features to your drive.

  • Advantages for Energy Management

    • Manage braking energy

    • Smoothing of DC bus voltage (in here from now on called DC link voltage)

    • Increasing energy efficiency (up to 25%)

    • Enhancing productivity (up to 50%)

    • Compensation for voltage dips

    • Bridging power failures

    • Controlled stops in case of power outage

    • Reducing peak loads on the power grid

  • Safety Features

    • Reverse polarity protection for intermediate circuit

    • Integrated pre-charging

    • Charging protection switch

    • Integrated load monitoring on both sides

    • Internal fuses

  • Extensions

Plug-On module PxtMX

Layout and Sizing

The layout and sizing can be done in cooperation with Koch Bremsenergie (Contact Information).

In order to find the best solution, it will be beneficial to provide some data depending on the use case.

Furthermore, the layout-portal can be used to gather some initial information.

Here is a detailed list of which data one should prepare:

  • In General

    • Limit current / power from grid

    • Grid topology (voltage, phase number, frequency)

    • Energy of load peaks / load cycle

    • Infeed rectifier (XCS, XVE) / active front end (XVR)

    • Intermediate circuit capacity

    • Connection cable length (Converter and PxtFX / PxtRX)

  • Recuperation

    • Max. braking power

    • Braking time

    • Braking power curve over time (block / ramp)

    • Cycle time

  • Load peak reduction

    • Average power demand

    • Max. power demand and peak load

    • Duration of load peak

    • Load peak curve over time

    • Cycle time of load peak

  • Short-term UPS (uninterruptible power supply) (German: USV)

    • Max. power demand

    • Support time ("Stütz-Zeit")

    • Power demand curve over time (block / ramp)

    • Cycle time

You can use several options to generate a power-time-diagram:

In general, a power-time-diagram will be sufficient. (Mains Power: P-0-0382.0.0)

Connection

The Koch Module has several different connections that will be shown in the following diagram:

Koch Module PxtFX

Further technical details are available on the product webpage.

The connection itself is quite simple.

One can easily connect the Koch Module to the intermediate circuit of the drive. There is no further configuration needed.

In the following image, which is taken in Ulm, one Koch-Module (red) and two Supercaps (black) are visible:

Koch Module installed in the Control Cabinet

Control Strategy

Short-term UPS - Functionality

The Koch Module is used to protect the application against short-term grid power faults. Define an UPS voltage level (e.g. 470 VDC) which the company Koch will parametrize inside the module.

If the voltage is above 470 VDC, the drive system will be fed by the power from the grid. In case of power interruption, the DC-bus voltage decreases. If the voltage would go below 470 VDC, the Koch Module will power up the DC-bus and stabilize the voltage level as long as energy is available. The Koch Module will start to recharge itself when a defined DC-bus voltage is reached.

UPS application

Manage Braking Power

The Koch module can be efficiently used to manage braking power. The braking power of a drive, which normally would dissipate into heat and be wasted, can be saved by an energy storage system.

The Koch Module provides two working principles:

a) Set a fixed DC-bus voltage level (e.g. 730 VDC) to activate and deactivate the Koch Module

When the DC-bus voltage exceeds 730 VDC, the Koch module starts to take energy out of the DC-bus with a current/voltage-ramp of 1 A/V.

If the Koch Module's power is not enough, and the DC-bus power is still increasing, the Koch Module increases the current with 1 A/V. (E.g. 735V = 5V difference -> 5A).

When the voltage decreases and gets below 730 VDC, the Koch Module will be discharged and stabilize the DC-bus voltage with a current/voltage-ramp of 1 A/V.

b) The Koch Module is triggered by brake off chopper-signal

The Koch Module will be triggered by BRC signal (brake chopper off signal) in this case. It will be in teaching mode and automatically set the DC-bus voltage level to 40 VDC below the chopper-off-voltage-level. Activation and Deactivation of the Module will behave exactly like in case a).

Example: Chopper off voltage level = 770 VDC -> After some cycles, the Koch Module will be activated by 730 VDC with storage current per DC Bus voltage difference of 1 A/V (PxtFX).

-> In this mode, the Koch Module will set the DC-Bus voltage level to max. 760 VDC.

Brake-Chopper-Operation and Pxt-Operation

Peak power shaving with active front end power supply XVR

The use of active front-end inverters enhances functionality. XVR offers features such as infeed current limitation (power limitation) and regenerative current limitation. Hence, the Koch Module can provide peak power shaving functionality.

Example: The application needs 160kW peak power on DC-bus and the connected Koch Module can provide 40kW peak which reduces the necessary power supply to 120kW. In result, the infeed current can be limited to 173A (120kW at a three-phase 400 VAC supply).

The same procedure is possible for regenerative power to the grid.

Power control with Koch PxtMX communication module

Using the Koch PxtMX communication module, the system can be controlled via EtherCAT, enabling cyclic command value control of the Koch Modules. This will provide more flexibility in power and energy control.

Requirements of Use

For more details on technical data, visit the company website or reach out directly to a Koch team member.

Exemplary Topology

Exemplary Network Topology

Related Links

The Company

Michael Koch GmbH, located in Ubstadt-Weiher, Germany is a producer of active energy management systems and safe brake resistors for Electric Drives.

Maximize your energy efficiency whilst increasing the performance of the electric drive technology, reduce the connected load and increase the reliability in case of voltage fluctuation or failure of the grid.

2
Types
How-to
Products
Drives
Markets
Semicon & Electronics
Manufacturing
Assembly Lines
Logistic
Production Machines