Version 1.2603.08 (2026-06-01)
Features
ctrlX DRIVE XCS2-L
ID 1194251
To enable users to select just the XCS2-L without the corresponding MS2L servo motor and cables, the add products now contains a stand alone product configurator for the drive.
ctrlX I/O: XI510004, XI541101
ID 1147920
The product configurator for ctrlX I/O now includes the new communication modules XI510004 and XI541101.
ctrlX DRIVE - capacity module
ID 1162887
The new capacity module R911427942 XLC1-W02M2-A-0750-NN is now available in the corresponding product configurators for ctrlX DRIVE.
ctrlX DRIVE - Sytronix SvP
ID 1176502
The ctrlX DRIVE product configurator now supports the combination of Sytronix SvP and Technology Function TX1.
ctrlX DRIVE cabinet free
ID 1176503
The product configurator for ctrlX DRIVE cabinet free has been extended by coldplate single axis drives.
ctrlX DRIVE - XCS2-H/XCS2-L 3D Previews
ID 1181377
The 3d previews in the product configurators for ctrlX DRIVE XCS2-H and XCS2-L have been updated by new previews to better visualize the product.
ctrlX DRIVE cabinet free
ID 1186879
The product configurator for ctrlX DRIVE cabinet free has been extended by 16 and 30 A air cooled double axes drives.
New features in the configurator ctrlX IPC PR5x.2 Box PC
ID 885089
The G1 software components for IndraWorks HMI Visualisierung (ML*) and IndraWorks CNC Visualisierung (MTX) have been added to the ctrlX IPC PR5x.2 Box PC configurator.
New features in the configurator ctrlX IPC PR4x.2 Box PC
ID 983858
The G1 software components for IndraWorks HMI Visualisierung (ML*) and IndraWorks CNC Visualisierung (MTX) have been added to the ctrlX IPC PR4x.2 Box PC configurator.
Updated Price Sheet for sales
ID 1024262
A new version of the price sheet for sales has been implemented. This includes better error handling and more enhanced information about missing data.Â
ctrlX I/O - Bit width
ID 1112222
The ctrlX I/O configurator now displays the needed bit width for each module and sums the bit width up in the station details.
New features in the configurator ctrlX IPC PR4x.2 Box PC and CtrlX IPC PR5x.2 Box PC
ID 1139201
The value "with Nvidia GPU Extension" have been added to the characteristic "Hardware Proberties".
Resolved Bugs
Gearboxes GTMxx2 - 3D preview
ID 1170329
The 3D preview only shows one configuration and not any hardware differences depending on the selection.
Materialnumer for cable
ID 1145035
For RLC1 cable connections the material number is missing in product configuration and list view.
Translation and textual errors
ID 1190221
In the ctrlX I/O configurator the texts and translations for the complete I/O portfolio contains several errors.
MSM incorrect dimensions
ID 1191526
The MS2M31C dimension view contains incorrect dimensions for the length.
ctrlX MOTION HMI license selection
ID 1209920
When trying to select one single ctrlX MOTION HMI license the configurator shows the incorrect configuration.
Standstill current in MS2* configurator
ID 1220393
In the product configurator of servo motor MS2* the configurator shows incorrect values for Standstill current 100K.
Information text for SIL3
ID 1220397
The information text for SIL3+ is missing in the ctrlX DRIVE product configurator attached to the corresponding characteristic.
Version 1.2603.05 (2026-04-08)
Features
Search Bar Added for Faster App and License Selection in the App Configurator
ID 974811
A new search bar is now available in the App Configurator, making it easier and faster to find apps and licenses. The search supports partial matches, is case‑insensitive, and filters results instantly as you type. It integrates seamlessly with existing data loading, helping users quickly locate the correct selectable options and improving overall efficiency when managing app configurations.
Discount Input Added to the New List View
ID 998841
The new List View now includes a dedicated Discount input field, allowing users to enter percentage based discounts directly at the item/group level. The Discount Price and Total Net Price columns update automatically, reflecting the applied discount and final net value.
Group level discount behavior has been refined for clarity and consistency:
Setting a Group Header Discount applies that percentage to all items in the group.
Adjusting an individual item’s discount switches the Group Header Discount to -%, indicating mixed values.
Reapplying a Group Header Discount updates all item level discounts to match the new group value.
ctrlX MOTION HMI
ID 1176510
License for ctrlX MOTION HMI is available in the app configurator.
ctrlX CORE in ctrlX DRIVE - App configurator streamlined
ID 1171945
Streamlined App Configurator in ctrlX DRIVE.
Update of MS2E product configurator
ID 1163884
The MS2E product configurator has been updated.
Streamlined CAD Format Selection for Faster, Simpler Downloads
ID 1162959
The CAD download dialog has been simplified to help users quickly choose the correct file format without navigating outdated or unnecessary options. Legacy formats have been removed, and only supported formats are now shown directly on the first level. The Options button has been removed, and the previously available formats (Creo, IGES, VDA, Catia V5, SAT, and SOLID MODEL) are no longer displayed. This update reduces confusion, speeds up selection, and ensures users only see valid, supported CAD formats.
Discontinuation of ctrlX DRIVE with ctrlX CORE
ID 1156189
Discontinuation of ctrlX DRIVE Runtime Version 04 with Integrated ctrlX CORE will be discontinued and is not available in ctrlX Configurator anymore.
ctrlX DRIVE Accessories: Introduction of new mains chokes XNL1
ID 1147621
New XNL1 Mains Chokes Available.
ctrlX MOTION Improvement
ID 1147819
In the app configurators there are improved Motion areas. This includes showing all software licenses from other areas which are relevant for Motion applications.
DC bus connection set for coldplate
ID 1127094
DC Bus Connection Sets for Coldplate Devices are available in the drive configurator.
Update RKB, RKG and RLK cables
ID 1127247
New RKB, RKG and RKL cables were added.
Coupling of IndraDrive Mi with ctrlX DRIVE Now Possible
ID 1130624
It is now possible to couple IndraDrive Mi near-motor and motor-integrated servo drives (KSM02, KMS02, KMS03) with a cabinet-based ctrlX DRIVE power supply.
ctrlX DRIVE MS2L03-06
ID 1077582
New MS2L Servo Motors Available.
ctrlX DRIVE XCS2-L
ID 1077969
XCS2-L Drive Now Available.
Improved Connection Naming for Clearer Product Relationships
ID 857259
The ctrlX Configurator now displays clearer and more informative connection names. Each connection label includes the names of the two products it links by default (users can rename the connection if needed), making it easy to understand which items are connected at a glance. This enhancement improves transparency, reduces confusion, and helps users quickly identify product relationships within a configuration.
Improved CAD File Download: Email Delivery for Partial Success and Error Notifications
ID 1096705
CAD downloads are now more reliable, successful files are emailed even if some products fail, and errors are reported in a separate email. During processing, the Download CAD Files button is briefly disabled to prevent repeated requests.
Resolved Bugs
ctrlX DRIVE - Behaviour of the fieldbus slider
ID 544461
The slider for changing the length of the fieldbus between ctrlX DRIVE behaves in the area of maximum values not as expected.
Connection to user defined products
ID 912372
When connecting products to an user defined product, in some cases the connection type cannot be selected or changed.
Connections between some XMD2 and XVE2 not possible
ID 1031032
In some cases it is not possible to connect some XMD2 to XVE2, in these cases a loading spinner appears that does not disappear again
Customer Number Reset with Global List Price
ID 1087768
An issue has been resolved where the customer number was being reset in the project settings when using the global list price.
Connection Enabled for MS2N10-E0BHA and XMS2-W0090
ID 1089889
It is now possible to connect the MS2N10-E0BHA with the XMS2-W0090. The required cables for this connection are now available for selection.
MAD Product Variant Added to Configuration
ID 1090030
The missing MAD motor product variant (R911429985) has been added to the MAD configuration, allowing it to be connected to the ctrlX DRIVE.
Checkbox for Separate Encoder/Power Cable Added
ID 1119087
The checkbox for selecting a separate length encoder/power cable is now available for connections between ctrlX DRIVE-A and MAD/MAF, as well as XCS2-F/H and MS2M.
Improved Configuration Stability and Validation
ID 1123248
Various issues related to updating, validating, and starting a configuration have been addressed. This includes fixing a problem where defaults were not being set correctly after starting a product configuration via "DISASSEMBLE TYPECODE".
System stops while connecting products
ID 1144717
The platform stopped working while connecting products on the graphic view.
Corrected Profibus Option Availability
ID 1148718
An issue has been fixed where the Profibus option was incorrectly available for HCS01 in AV. It is now correctly restricted to SV products only.
Connection Between XMD3636 and MS2N10 Now Possible
ID 1149470
An issue preventing the connection of XMD3636 to MS2N10 has been resolved.
Show Details Now Accessible for All User Roles
ID 1155644
An issue preventing distributor-level users from accessing the full "Show Details" panel for certain products has been resolved. The panel now populates correctly for all user roles.
MLP Product Variant Now Available via Product Search
ID 1157666
The MLP product variant R911324384 can now be successfully added to the graphic view from the product search and configured.
Resolved Issue with Adding MAD Products
ID 1159940
An issue that prevented some MAD products from being added to a configuration has been fixed. Products from the search can now be added as expected.
Updated Description for Onboard Extension on ctrlX Core
ID 1160704
The descriptive long text for the "Onboard extension" characteristic has been updated to provide clearer and more accurate information.
Missing GTE Gearbox Variants Now Available
ID 1162401
Missing GTE gearbox variants (e.g., GTE120-NN1-004B-NN20, GTE120-NN2-040B-NN20) have been added to the configurator and are now available for selection.
Additional Gearbox Combinations Now Available
ID 1162755
An issue preventing certain gearbox combinations from being added as configurable products has been resolved. These products can now be added and configured correctly.
Material Number Now Displayed for IndraDrive Mi KSM02
ID 1163191
An issue where the material number was not shown for IndraDrive Mi KSM02 (R911372926) after being added via product search has been fixed. The material number is now correctly displayed.
Encoder emulation with double axes devices
ID 1165471
Encoder Emulation Now Possible with Double Axes Devices.
RL2 Can Now Be Added to Topology
ID 1172839
An issue preventing the RL2 cable from being added to the topology has been resolved.
Connection Enabled for MS2N07-D0BHA and XCS2-W0054ARN
ID 1172841
An issue preventing the connection between the MS2N07-D0BHA motor and the XCS2-W0054ARN drive has been fixed. These components can now be connected.
Missing Gearbox Characteristics Now Included
ID 1176414
An issue where some gearbox characteristics were missing when requesting CAD details has been resolved. All characteristics are now correctly included.
Links for further documentations adds WeidmĂĽller app even if not configured
ID 1176975
Corrected Links in Project Documentation.
Regenerative Power Supply Selection Limited by Voltage
ID 1178309
The selection of a regenerative power supply is now correctly limited by the mains voltage range to prevent invalid configurations.
Material Numbers Now Displayed for More Products
ID 1181850
Issues preventing material numbers from being shown for several products, including certain gearboxes and IndraDrive Mi variants, have been resolved. Material numbers are now displayed correctly.
ctrlX I/O modules - amount in 3D different to quantity
ID 1183845
Corrected Quantity of ctrlX I/O Modules in List View.
Corrected Dependency for Connector Set in ctrlX DRIVE - A
ID 1186177
The dependency for the connector set in ctrlX DRIVE - A has been corrected to align with the product documentation, ensuring valid configurations.