12/16/2025
Technote | ctrlX Configurator | Release notes

ctrlX Configurator - Release Notes version 1.2511.18

Version 1.2511.18 (2025-12-11)

Features

  • Usability Improvement: Flexible Save Options for Projects
    ID 858068
    To improve usability, users can now save their ctrlX I/O or ctrlX FLOW HS projects without interrupting their workflow. Instead of forcing the page to close and requiring re‑entry into edit mode, the new save behavior allows projects to be saved directly while continuing to work on the canvas or configuration. Clear feedback is provided through a toast notification confirming that the project has been successfully saved, while additional options remain available to either close without saving or save and close to return to the main page.

  • Text boxes and Shapes
    ID 710114
    Within the graphic view there is now the possibility to add visual text boxes and rectangles to improve the layout visibility.

  • Gearboxes GTE & GTMxx2
    ID 428323
    ctrlX Configurator now supports a separate product configurator for gearboxes of the families GTE & GTMxx2.

  • Multi-Tab Support
    ID 612305
    Users can now open and use the Platform in multiple browser tabs without triggering page refreshes.

  • Linear motors - MCL
    ID 633953
    ctrlX Configurator now supports the products Linear Motors of the Line MCL. The product configurator is available and the products can be connected on the topology.

  • Labels for Connections
    ID 839598
    Activating Show cable labels in Project Settings and Filters displays labels for every connection in the graphic view. The topology becomes easier to interpret through clear visibility of each connection´s category.

  • Module Name Character Limit in ctrlX I/O
    ID 841581
    The platform now enforces a maximum of 25 characters for module names in ctrlX I/O projects, ensuring consistency with FLOW HS product behavior in the Configurator. If a user enters a name longer than 25 characters, the system displays an error message with feedback to create a shorter, valid name.

  • Unique Module Naming in ctrlX I/O
    ID 843624
    The Platform now enforces unique names for modules in ctrlX I/O projects, ensuring consistency with the FLOW HS product behavior in the ctrlX Configurator. When creating or renaming a module, the system checks for duplicates, prevents changes to existing production modules, and automatically appends "_copy" to avoid conflicts(This applies only to projects already in production with duplicated module names). Users receive error feedback if a name is already taken.

  • Improved Sidebar Usability in ctrlX I/O and ctrlX FLOW
    ID 850704
    The left Add Components/Segments and right Details sidebars in ctrlX I/O and ctrlX FLOW now offer enhanced usability. Both can be expanded or collapsed, giving users greater control over hiding or enlarging the panels. This update provides a more consistent and streamlined navigation experience across products.

  • IP65 cabinet free drive
    ID 799170
    The IP65 cabinet free drive XMD2 with 16A and 30A, the XCU1 Connection module, the XIU1 Interconnection unit and the XLT1 Topology node are now available.

  • Platform Upgrade: Java 21 & Tomcat 10
    ID 833890
    The ctrlX Configurator Platform´s Java runtime has been upgraded to Java 21, and the application server to Tomcat 10. This update delivers improved performance, enhanced security, and long term support. Compatibility and stability have been verified across all environments (Dev, Q, and Production).

  • Auto‑Save Available in Project Settings
    ID 903139
    A new Auto‑Save option in Project Settings enables automatic saving of project changes. The feature is turned off by default and can be activated at any time. Manual saving remains fully available, even when Auto‑Save is enabled.

  • New Filter Option: View Discontinued Products in ctrlX Configurator
    ID 906561
    A new filter, Show Only Sellable Product, has been added to ctrlX Configurator. Enabled by default, it displays only current sellable products. Internal users can now toggle this filter off to view both sellable and discontinued service products. When visible, discontinued service products are clearly marked with an SV icon for easy identification.

  • ctrlX OS licenses delivered on license dongle
    ID 909521
    It is now possible to deliver the selected ctrlX OS licenses on a license dongle. The license dongle is displayed as part of the ctrlX CORE configuration, but is an integral ctrlX accessory that can also be ordered separately.

  • Connection XCS2-F to MS2M
    ID 915506
    The connection configurator between XCS2-F and MS2M has been extended to enable the configuration of a length up to 30 metres.

  • Product data base update
    ID 955561
    For several products the data base has been updated and extended, e.g. MAD, MAF and EFC.

  • ctrlX DRIVE compact - XCS2-H
    ID 960745
    ctrlX Configurator now supports the product line ctrlX DRIVE compact XCS2-H. The families portfolio can be configured and connected on the Graphic View.

  • ctrlX DRIVE - Default encoder setting
    ID 964801
    The default of the device configuration within ctrlX DRIVE has been changed to "without EC".

  • ctrlX Apps | Streamlining apps configurator
    ID 974808
    The configurator for ctrlX OS and Partner Apps in ctrlX CONFIGURATOR for ctrlX CORE and ctrlX Apps are improved. The configurators now has an optimized view with subheadings, indented areas and a simplified overview of the individual apps.

  • Material Variant Number Added to XML Output
    ID 984076
    The XML file generated by the ctrlX Configurator now includes the material variant number when available. If no material variant is found, the ZKMA number and its items will be used instead.

  • Multi ZKMA Support in ctrlX CORE Configurator
    ID 984430
    The ctrlX CORE Configurator now supports multiple ZKMAs within a single product setup. This enhancement enables configuration of license dongles with onboard licenses, providing greater flexibility and efficiency in license management.

  • Performance improvement for Data
    ID 1000534
    To improve the performance and stability with showing data for example in the area of "Show details" and Product Catalogue, the data provision has been changed to a separate API.

  • Auto save with CAD Download deactivated
    ID 1010990
    To improve saving of projects and usability for users the automatic Save of projects when downloading CAD has been deactivated. As of users feedback this led to a lot of unneeded project saves.

  • ctrlX DRIVE - MS2 with Gearboxes*
    ID 1022918
    In the product based configurator of the Synchronous servo motors the gearbox characteristics are now hidden as long as no gearbox is selected.

  • ctrlX CORE | New extension module for ctrlX CORE
    ID 1024406
    New ctrlX CORE extension module "AI Module" can be selected as part of ctrlX CORE plus with performance class "X3".

  • ctrlX CORE - AI module for performance classes "X5" and "X7" integrated
    ID 1026067
    The option "AI Module" for "OnBoard Extension 1" can now be selected with "Performance class/category" within "X5" and "X7".

  • Update of IndraDrive Cs - HCS01 configurator
    ID 1032194
    The HCS01 product configurator has been updated to match all relevant product variants.

  • ctrlX DRIVE - MS2E motors
    ID 1042596
    The ctrlX DRIVE MS2E Ex protected synchronous servo motors are now available as a separate entry in the add products dialogue.

  • ROKIT motor
    ID 1043136
    ctrlX Configurator now supports the ROKIT motor and enables the connection to needed devices on the graphic view.

  • IndraDrive Mi - Accessory defaults
    ID 1043142
    To improve the product configurator for IndraDrive Mi the defaults of the accessories have been reworked to include the mounting brackets by start.

  • IndraDrive Mi - Accessory IO cables
    ID 1043145
    In the IndraDrive Mi connection configurator the option "Cable for digital IOs X37, X38" is now available to include the corresponding accessory.

  • Selection of safety functions in ctrlX DRIVE
    ID 1045640
    Due to a potential misunderstanding of users, the selection of safety functions needs to be reworked. The order of the characteristic values of the characteristics "SAFETY CTRLX DRIVE" and "FUNCTIONAL SAFETY CTRLX DRIVE" were changed.

  • Update ruleset for ctrlX OS - ROKIT Locator Client
    ID 1048247
    New dependencies for ctrlX OS - ROKIT Locator Client is implemented. The license no longer can be selected in ctrlX DRIVE integrated CORE´s and not can be configured in ctrlX CORE plus within performance class X3.

  • New ctrlX I/O Module XI482204 integrated
    ID 1053442
    The new ctrlX I/O Module XI482204 is integrated in the ctrlX I/O configurator and can be selected.

  • Connection for MS2N & MS2S and XCS2.F and XCS2-H
    ID 1053445
    New cables have been added to connection configurator to enable connection for

    MS2N & MS2S and XCS2.F and XCS2-H.

  • ctrlX CORE | Power over Ethernet Switch as accessories part of ctrlX CORE
    ID 1053451
    A Power over Ethernet Switch can now be selected as accessories part of ctrlX CORE in ctrlX CORE configurator.

  • ctrlX DRIVE - New mains filter XNF1
    ID 1053424
    The mains filter XNF1 with 12A/70nF and 80A/290nF were added for the ctrlX DRIVE.

  • ctrlX I/O new modules
    ID 1077587
    The ctrlX I/O configurator now supports the following new I/O modules - XI113208, XI233204, XI234204, XI382204.

  • ctrlX Apps | "Bosch Rexroth - ROKIT Locator Client" in ctrlX Apps and ctrlX CORE CONFIGURATORS
    ID 1078981
    New license "ctrlX OS License - ROKIT Navigator" is integrated in within ctrlX Apps and ctrlX CORE Embedded Control configurator.

  • Enhanced List View: Create Multiple Groups
    ID 1082732
    The List View now supports creating more than two groups, removing the previous limitation of only two. This update allows for greater flexibility in organizing items into customized categories, helping users manage and reorganize their List View more efficiently.

  • Global Control of Price and Delivery Visibility
    ID 1085147
    Users can now manage the visibility of List Price, Net Price, and Delivery time across the entire platform. These toggles now impact all views and tools, including the List View, Product Details, Product Search, Product Configurator, Download files, and summary values (sum list price and sum net price).

  • Distribution partner in Sweden
    ID 1085433
    Correction of data for distribution partner in Sweden.

  • Linear motor ML3
    ID 1097205
    The product configurator ML3 has been updated to match the new product variants.

  • Further hardware configurations
    ID 1106125
    Further hardware configurations with more than one extension are released for the ctrlX CORE X5/X7. For COREplus X5/X7, up to 3 extensions are allowed.

  • ctrlX OS HSR/PRP License
    ID 1106130
    ctrlX OS HSR/PRP License for secure and redundant network communication supporting ring (HSR) and parallel (PRP) topologies. HSR and PRP provide seamless failover against failures in one of the network components.

  • ctrlX OS License - Firewall Basic
    ID 1106133
    The Firewall App is an industrial firewall for ctrlX OS. The firewall inspects traffic between networks based on predefined criteria. The data packets are either accepted or blocked. It is based on Nftables technology and supports Network Address Translation (NAT). The Firewall app is used to protect the machine from unauthorized network access by users or viruses.

  • ctrlX Apps | "CODESYS - PLC Add-ons - WebVisu and CANopen" in ctrlX Apps and ctrlX CORE CONFIGURATORS
    ID 1106136
    New license for "CODESYS - WebVisu" and "CODESYS - Fieldbus Communication" (CANopen) are integrated within ctrlX Apps and ctrlX CORE Embedded Control configurator.

  • New features in the configurator ctrlX IPC PR2x.2 Box PC
    ID 1106969
    The new feature value "with Win11 IoT 2024, Entry" have been added to the ctrlX IPC PR2x.2 Box PC configurator.

  • Dependency of license model ctrlX MOTION implemented
    ID 1117113
    When Cam is selected, Electronic Gear is now also automatically selected.

  • ctrlX CORE and ctrlX I/O changed End Brackets in configurators
    ID 1121318
    Due to a change other End Brackets in ctrlX CORE and ctrlX I/O configurator are needed. Now "SUP-M01-ENDHALTER" instead of "SUP-M01-ENDHALTER/PA" are chosen.

  • New capacity modules XLC1 with 5mF
    ID 1121256
    The capacity module XLC1 with 5 mF were added to the ctrlX DRIVE configurator.

  • CAD available XAS2
    ID 1121493
    CAD files for the XAS2-008 and XAS2-009 can now be requested.

  • ctrlX DRIVE XCS2-F - remove hint
    ID 1122268
    A hint in the ctrlX DRIVE XCS2-F configurator was removed.

  • Update of MAD/MAF configurator
    ID 1127225
    New RKB, RKG and RKL cables were added.

  • Update of ML3 configurator
    ID 1127238
    Additional materials added as a result of cleanup analysis, EPLAN for ML3 deactivated in CPQ.

  • Update RKB, RKG and RLK cables
    ID 1127247
    New RKB, RKG and RKL cables were added.

Resolved Bugs

  • Calculation of Required Power for 24V
    ID 1086057
    Calculation of required power for 24V not correct, because the brake is not considered. Rename "Leistung/power" in "Dauerleistung/..." and consider "Spitzenstrom/..." ctrlX DRIVE in the details section.

  • List View Sorting
    ID 1055204
    When switching between list- and graphic view the manual sorting of list view items get's returned to a default sorting.

  • Material Number in I/O Configurator
    ID 1074969
    Some characteristics of IndraControl XM42 are not shown in project summary under the headline "Features".

  • ZKMA Configuration Conflict
    ID 1097404
    When selecting ECEC and DL, the ZKMA configuration runs into a conflict.

  • Additional Cable for XLI Bus Communication
    ID 1099960
    For the connection between XVR2 and XLI a firewire cable RG2 is required. If a customer cannot place XVR2 and XLI beside each other, an additional cable can now be selected.

  • Encoder Cable Length Selection Missing
    ID 1100496
    Option to select a different length for encoder cable is missing when connecting

    XCS2- with MS2M.

  • XCS2-F Multi Ethernet Cable Connection
    ID 1100532
    After deselecting the mains filter the respective XCS2-F can not be connected to another XCS2-F via multi ethernet cable although they should have the same communication protocol.

  • EFC Frequency Converters Default
    ID 1102628
    The initial default is changed to products with operating panel = 7-segment LED display (7P).

  • MS2N Motor Connection
    ID 1102630
    Not possible to connect MS2N07-E0BNL together with XMS 90 Amp - now resolved according to documentation.

  • Save Project Indicator
    ID 1105154
    Save project bubble indicator color issue resolved. Bubble now stays green after switching between graphic view and list view when project is saved.

  • Motor Cable for XMS2-W0090
    ID 1088471
    Motor cable for XMS2-W0090 not found in configurator - now resolved.

  • Error Message PDCcont
    ID 1110316
    The error message now only appears for DC bus connections, not for fieldbus connections. Only DC bus connections should trigger the drive line calculation.

  • ZKMA Communication EX
    ID 1110374
    ZKMA does not allow communication EX (ctrlX OS) with runtime 05 for affected products XMV2, XVE2, XVR2, XCS2, XCD2 - now resolved.

  • I/O Group Display
    ID 1115384
    In the I/O Group section: The bus coupler price is now correctly displayed, quantity shown correctly, and subtypecodes properly formatted.

  • Missing Checkbox for Connections
    ID 1119087
    Checkbox missing for connections ctrlX DRIVE-A - MAD/MAF, XCS2-F/H - MS2M - now added.

  • Project Validation Errors
    ID 1123248
    Various errors after validating a project resolved: Defaults now set correctly, wrong cable after validation fixed, blocked port properly removed after deleting a connection.

  • Power Supply Calculation for XVR2
    ID 1123580
    Power supply calculation for XVR2 corrected. The 24V control voltage power calculation is now accurate.

  • XCS2 Configuration
    ID 1124363
    R914521604 XCS2-W0100ABN-01NETTBECNN-S06RSN4TE0S0NN can now be configured.

  • Save Icon Behavior
    ID 1125694
    Save Icon changing issue resolved. The TopologyRowId for Fieldbus coupler EtherCAT is now maintained during solution loading.

  • PDCcont Calculation
    ID 1126899
    Wrong PDCcont calculation corrected. The "C_ab_cable_sum" characteristic is now displayed in the details section.

  • Connection Drawing Issue
    ID 1126931
    Connection drawing issue with specific motor configuration resolved. Connection can now be established properly.

  • Power Supply Error Message
    ID 1126932
    Error message "Power supply does not deliver enough power for the connected consumers" now appears correctly. Interpretation of SafetyLink connection versus DCBus connection corrected.

  • Type Code Display for KSM/KMS
    ID 1128846
    Type code of the KSM/KMS is now shown in the list view and in the details.

  • Drive and MS2N Motor Connection
    ID 1129730
    Connection between specific drives and MS2N motors now possible according to documentation.

  • HCS01 NFE Line Filter 1x 230 V
    ID 1133095
    HCS01 NFE Line filter 1x 230 V now available. Mains filter R911266399 - NFE02.1-230-008 added to configurator.

  • ctrlX CORE Safety Configuration
    ID 1134182
    The combination ctrlX CORE (X3) with Hardware option 1 - Safety = SafeMotion - I/O's & Fieldbus (M8) can now be selected in the ctrlX DRIVE configurator.

  • IndraDrive Mi Type Codes
    ID 1137315
    Type codes for IndraDrive Mi products (KMV03, KSM, KMS02/03) are now shown in List View.

  • XVR2 Error Message
    ID 1138383
    Power supply XVR2 error message corrected. The allowed leakage capacitance calculation and C_ab_cable_sum characteristic display are now working properly.

  • ctrlX Dongle Display
    ID 1140057
    Configured ctrlX Dongle R914521723 now correctly displayed instead of showing R914521722.

  • Translation Functionality
    ID 1142091
    Translation now works when changing language.

  • Cable Details View
    ID 1142976
    Cable details view now shows complete information about connections as expected.

  • ctrlX I/O Price Calculation
    ID 979506
    When requesting prices in ctrlX I/O configurator in some situations the price is calculated for the incorrect quantity of modules.

  • ctrlX DRIVE Configuration
    ID 1031547
    When selecting a ctrlX CORE as part of an ctrlX DRIVE, it is not possible to deselect the ctrlX AUTOMATION - DRIVE Connect App.

  • XCS2-F Productivity Mode
    ID 1122032
    Within the XCS2-F product configurator when selecting productivity mode the configuration cannot be confirmed.

Types
Technote
Products
Services