03/12/2026
How-to | IoT | Controls

Connect to MySQL Server using Node-red and run MySQL locally on ctrlX CORE

Requirements:

  • ctrlX CORE X3/X5/X7 or ctrlX CORE Virtual with internet connection

  • Node-RED app

  • PLC app (optionally)

  • MySQL Server (on PC or snap)

  • Basic snapcraft knowledge

  • Configured Environment to build the snap

Set MySQL Server

You can download MySQL installer for your target platform or use portable .zip archive, I will use portable mysql-8.0.38-winx64 in this guide.

Jump in 'mysql-8.0.38-winx64\bin' folder with CMD

Use command to initialize the server:

mysqld --initialize --console

You will need to save the temporary password:

Initialize MySQL

Start server:

mysqld --console

You will see it running on port 3306:

Running MySQL

Now, run another terminal, go to the same directory and connect to the server:

mysql -u root -p

Successful connection log:

Connecting to MySQL

Optionally, we can change password now, I will change it to 'boschrexroth':

ALTER USER 'root'@'localhost' IDENTIFIED BY 'boschrexroth';

let's create a database:

CREATE DATABASE db1;

and switch to use it:

USE db1

You will get the response:

Create MySQL db

We are nearly good to go, just create a new user, grant permissions and use flush for immediate refresh of the rights:

CREATE USER 'ctrlxcore'@'10.195.70.29' IDENTIFIED BY 'boschrexroth';
GRANT ALL PRIVILEGES ON *.* TO 'ctrlxcore'@'10.195.70.29'WITH GRANT OPTION;
FLUSH PRIVILEGES;

if you get 'Query OK' after each command, can proceed further:

Create new user in MySQL

Install the node:

If you are using a Virtual core, like me in this guide, make sure that port forwarding is on, you also need to enable external access:

ctrlX CORE Virtual Settings

Run it!

Now we can set up Node-red, you will need to add "node-red-node-mysql" to your palette, just open for palette, search for it and press install, but make sure your ctrlX CORE has connection to the internet.

node-red-node-mysql

Configure the Flow:

Insert required nodes:

MySQL flow

  1. Edit settings of MySQL Server node to match the MySQL settings we've done before:

    MySQL node settings

  2. Make a script for creating a table in our Database:

    msg.topic= "CREATE TABLE Drives (id SERIAL PRIMARY KEY, device_id VARCHAR(50) NOT NULL, timestamp TIMESTAMP NOT NULL, velocity FLOAT, position FLOAT, torque FLOAT, status VARCHAR(20));"
    return msg;

  3. Script for inserting a table:

    msg.topic= "INSERT INTO Drives (device_id, timestamp, velocity, position, torque, status) VALUES ('HCS01', NOW(), RAND() * 1000, RAND() * 10000, RAND() * 20, 'OK');"
    return msg;

  4. Script to read data from table:

    msg.topic= "SELECT *From Drives;"
    return msg;

Now you can press first inject to create a new table:

Create a table

In MySQL terminal you can display created tables and get data from them:

SHOW TABLES;
SHOW COLUMNS FROM drives;

Result:

Tables in MySQL Server

You can delete table with command:

DROP TABLE drives;

Read data from PLC

Create a simple PLC program to create an array of values, I am using OSCAT library to randomize it:

PLC program

Don't forget to configure Symbol Configuration to publish your variable:

Symbol

Load the code to your ctrlX CORE.

We need to add 'Read Datalayer' node and modify our script:

Read from Datalayer

  1. Edit device settings and path to your variable:

Edit Datalayer node

  1. Insert the script, we only get torque value from PLC, other we keep randomized in Node-red:

    msg.topic = "INSERT INTO Drives (device_id, timestamp, velocity, position, torque, status) VALUES ";
    
    for (var i = 0; i < 998; i++) {
        var temp = msg.payload.value[i];
        msg.topic += "('HCS01', NOW(), RAND() * 1000, RAND() * 1000, "+msg.payload.value[i]+", 'OK'),";
    }
    msg.topic += "('HCS01', NOW(), RAND() * 1000, RAND() * 1000, " + msg.payload.value[998] +", 'OK')";
    msg.topic += ";";
    
    return msg;
    

Now after creating a table and pushing the data, you can check the tables using third inject:

Node-red table display

Or get it in MySQL terminal using 'SHOW COLUMNS FROM drives;' command:

Display columns in MySQL

Run MySQL on ctrlX CORE locally

Optionally, you can run MySQL Server on ctrlX CORE in a snap, please refer to official Canonical Github webpage for MySQL source code, it's easy to find. First you will need to change base version from core24 to core22 (if you are using Ctrlx OS 2.X.X/3.X.X), change mysql-server stage package to match it and build the snap. Install it on your ctrlX CORE:

MySQL snap

You will need SSH access to the ctrlX CORE for initial setup. After accessing the ctrlX CORE, you can check available commands:

ls /snap/bin/ | grep mysql

Create a new password:

sudo mysql.mysqladmin -u root password 'boschrexroth'

And access MySQL server:

sudo mysql -u root -p

Your terminal should look like this:

SSH access

After that we can use standard commands to create a new user, you already know how to do it, just use localhost IP. Change the settings in Node-RED and enjoy the result!

MySQL snap connection

You can automate user and database creation by modifying install hook 'snap/hooks/install', just extend the script with custom function, for example new user ctrlxcore_auto and database db1:

create_app_db_and_user() {
    local init_file="$(mktemp)"

    # Create database
    echo "CREATE DATABASE IF NOT EXISTS db1;" >> "$init_file"

    # Create user with password
    echo "CREATE USER IF NOT EXISTS 'ctrlxcore_auto'@'127.0.0.1' IDENTIFIED BY 'boschrexroth';" >> "$init_file"

    # Grant all privileges
    echo "GRANT ALL PRIVILEGES ON *.* TO 'ctrlxcore_auto'@'127.0.0.1' WITH GRANT OPTION;" >> "$init_file"
    echo "FLUSH PRIVILEGES;" >> "$init_file"

    echo "SHUTDOWN;" >> "$init_file"
    chown snap_daemon:root "$init_file"

    # Run init file
    $SNAP/bin/setpriv.sh $SNAP/usr/sbin/mysqld \
        --defaults-file=$SNAP/etc/my.cnf \
        --user=snap_daemon \
        --skip-networking \
        --skip-mysqlx \
        --init-file="$init_file"
}

And run the function in the end of install hook:

create_app_db_and_user

Rebuild and install the snap, now you don't need any SSH access anymore!

Beware it is not recommended to use internal memory for deployment due to the limited capacity and lifetime of the memory!

Adding External Memory to Virtual CORE

For production purposes we will need to update the project to work with external memory.

This step can be skipped if you are using the real CORE.

If you want to use it on Virtual ctrlX CORE, you will have to replace drivers to make it accessible in QEMU emulator, one of the ways is to use Zadig software. Run it, select your USD Drive and click on "Replace Driver"

Driver Installation

Locate the Virtual image launch script and make a copy:

Virtual Image .bat

Edit it to make your USB Drive available in Virtual CORE, change vendorid and productid depending on the USB ID displayed in Zadig software:

-device qemu-xhci,id=xhci^
-device usb-host,vendorid=0x0930,productid=0x6545 ^

Save and run your control directly from a .bat script.

Memory mounting

Format the memory if needed and mount it for data exchange in Settings>Storage page:

Mount the memory

Now you can use /media/sdb1 link for your snap.

Source code modification

Modify 'snapcraft.yaml' to add 'removable-media' and 'hardware-observe' plug to mysqld apps section:

  mysqld:
    command: bin/mysqld.sh
    daemon: simple
    plugs:
      - network
      - network-bind
      - removable-media
      - hardware-observe

Locate 'snap/local/bin/mysqld.sh' and add code to use external media if available:

#!/bin/bash

INTERNAL_DATA="${SNAP_COMMON}/data"
EXTERNAL_DATA="/media/sdb1/data"

# If external media is accessible and data hasn't been migrated yet,
# copy the initialized database from internal to external storage.
if [ -d "/media/sdb1" ]; then
    if [ -f "${INTERNAL_DATA}/mysql.ibd" ] && [ ! -f "${EXTERNAL_DATA}/mysql.ibd" ]; then
        mkdir -p "${EXTERNAL_DATA}"
        chmod 775 "${EXTERNAL_DATA}"
        if "${SNAP}/usr/bin/setpriv" \
                --clear-groups --reuid snap_daemon --regid root \
                -- cp -a "${INTERNAL_DATA}/." "${EXTERNAL_DATA}/"; then
            chown snap_daemon:root "${EXTERNAL_DATA}"
            chmod 700 "${EXTERNAL_DATA}"
            # Clean up internal data only after successful copy.
            "${SNAP}/usr/bin/setpriv" \
                --clear-groups --reuid snap_daemon --regid root \
                -- rm -rf "${INTERNAL_DATA:?}/"*
        fi
    fi
fi

# Use external datadir if available, otherwise fall back to internal.
if [ -f "${EXTERNAL_DATA}/mysql.ibd" ]; then
    DATADIR="${EXTERNAL_DATA}"
elif [ -f "${INTERNAL_DATA}/mysql.ibd" ]; then
    DATADIR="${INTERNAL_DATA}"
else
    echo "ERROR: No initialized MySQL data directory found." >&2
    exit 1
fi

exec "${SNAP}/usr/bin/setpriv" \
    --clear-groups \
    --reuid snap_daemon \
    --regid root \
    -- \
    "${SNAP}/usr/sbin/mysqld" --defaults-file="${SNAP}/etc/my.cnf" --datadir="${DATADIR}"

Now you can rebuild and install the snap. You can check if data folder is moved to your media:

USB Drive data folder

Have fun using it!

Related Links:

MySQL :: MySQL Downloads

GitHub - canonical/mysql-snap: MySQL snap

IIoT: Use ctrlX CORE as a monitoring platform using InfluxDB and Grafana

GitHub - boschrexroth/ctrlx-automation-sdk: ctrlX AUTOMATION Software Development Kit

Get started with snaps | Snapcraft documentation

mysql_drives.json
5.58KB
mysql_drives_datalayer.json
6.48KB
Types
How-to
Products
IOT
Controls
PLC