Hi everyone,Â
I am testing to connect the ctrlX CORE X3 (as PROFINET Controller) to the Siemens PLC S7-1200 (as PROFINET Device). A customer of mine wants to collect the data from the S7, then synchronize it to the datalayer on ctrlX.
I have completed the following steps:
1. Installed all the required add-ins on my ctrlX CORE (Ubuntu Core 22).Â
2. Defined the IPs for both devices as the following: ctrlX CORE (XF10: 192.168.0.123) and S7-1200 (192.168.0.133). Both devices are wired through a switch with IP: 192.168.0.100.
3. Install the GSD file of the S7 into the ctrlX's device repository.
On the ctrlX CORE, I have setup the PROFINET Device through Codesys as the following. At this step, my ctrlX CORE has been able to scan the PLC S7-1200 and "Copy to the project" that device.
However, when I compiled the PLC program and login the ctrlX CORE, it could not make a connection with the S7 and kept showing the error "DB814006 - Connect Parameter Error". From the S7 side, the PLC blinked Red as it could not connect to the ctrlX yet.
I want to ask for support and suggestions what should I do/check/modify to be able to create a successful connection between the 2 devices.Â
I am new to ctrlX CORE, so I deeply appreciate your support a lot. Please just let me know if I should provide any more information.
Thank you first!