cant generate CSR file for AWS IoT Core Client in Codesys

I am using the AWS IoT Core Client from the IIOT Library. I have the credentials and keys of the MQTT broker I want to connect to.

I need to create an CSR file in the PLC shell but the PLC shel is blank, see attachment. How can i create a CSR file without PLC shell?ย 

ย 

I got credentials (Root Certificate and public & private key) from the AWS. I need codesys to allow these credentials.

How can install the credentials in Codesys?ย 

Best reply by CodeShepherd

Is this still an issue or can this topic be closed?

View original
PLC shell blank.JPG
78.96KB
3 replies