The 36ZERO Vision Adapter app is a self-service connector between 36ZERO Vision's highly accurate optical quality inspection system and a device, running ctrlX OS.
[youtube src="https://www.youtube.com/embed/svwJ064QfZE?si=_gMOmgGiKGGtL6U2"]
By using our easy-to-use web platform, a quality inspection system can be set up in a short amount of time. With the help of the 36ZERO Vision Adapter app, our Vision software can communicate to the industrial world to:
Trigger any GenICam® compliant camera
Receive the correct configuration of parts to verify with the visual inspection
Send back results for performing actions for example discarding defective parts through a robot. Visualizing information in dashboards or storing it in long-term quality management systems
Allows automation of industrial processes with the drag & drop platform of ctrlX OS with various industrial players. The 36ZERO Vision Adapter app acts as a bridge between the industrial world, which is abstracted in the Data Layer from ctrlX OS, and the quality inspection system from 36ZERO Vision.
Features
The Adapter App provides the following information after each and every prediction to the DataLayer:
Write:
Verdict of AI based visual quality inspection, like identified scratches
Information of read-out Barcodes, DMCs, etc.
Providing image path with individualisable meta data
Read:
Trigger from PLC system
Comparison between identified part (presence and absence) and ERP system information
DMC, Barcodes etc. and provide information towards the DataLayer
Additional advantages
Multiple users allowed
User- & Role-Management
Product traceability with Batch Testing on historical images (on cloud and on premise)
Raw statistical data to process in multiple ways for e.g. CSV for PowerBI etc.
Power of AI quality inspection without relying on internet connection (on premise solution)
Our proprietary software can run on existing hardware. Contact us and find out more!
Interface
ctrlX and 36ZERO Vision Environment
Prerequisites
ctrlX CORE 3 to run 36ZERO Vision Adapter App
Linux based Industrial Computer for AI prediction on premise
>1sec prediciton time = Industrial-PC with i7 or i9 CPU, 16GB RAM
<50ms prediciton time = Industrial-PC, i7 or i9 CPU, 16GB RAM, 8 cores, Nvidia GPU A or T class
Support of any Gen<i>Cam compliant 2D-Cameras (Area Scan or Line Scan Camera) via a Gig-E or USB-3 connection
Depending on the Use Case all prerequisites can be provided by 36ZERO Vision or from one of our partners.
Support
Related Links
Curious?
You can test many apps free of charge with a virtual control system provided by ctrlX WORKS.
Just download ctrlX WORKS and follow this How-to
[link-button type="light" text="TRY IT NOW" target="_blank" href="https://community.boschrexroth.com/ctrlx-os-store-apps-oc2pqqwn/post/ctrlx-works-xOJLFLUiK4NGm5H"]
The Company
36ZERO Vision is an AI-based software solution for visual quality automation to identify characteristics, anomalies, missing parts and reading of industrial text, this increases transparency and productivity through the entire process of quality control.
1) Note on data protection: The email is sent directly to the partner company! This company is responsible for the processing of the data contained. Please read their data protection information before sending this email! Bosch Rexroth is not responsible for the use of the partner company's support.